<iframe src="//www.googletagmanager.com/ns.html?id=GTM-WHST8N" height="0" width="0" style="display:none;visibility:hidden">

Stay Powered Blog

Server Technology Solution Partner Providers

Posted by Calvin Nicholson on Mar 28, 2014 11:38:00 AM

Server Technology Solution Partner Providers (Part 1 of at least 2 Parts)


I always find it interesting that the power chain is measured and monitored in multiple locations throughout most data centers but is often forgotten once the power enters the data center cabinet. Especially considering that roughly half of the power used (or more) can be traced directly to the cabinet (See Figure 1) and power is typically one of the greatest single costs associated with operating a data center. Often monitoring at the cabinet is the invisible line between the IT and Facilities groups. Even though monitoring at the in-feed of the Cabinet Power Distribution Unit (CDU) is really the same as monitoring at the Remote Power Panel (RPP) as the branch circuits coming out of the RRP are the in-feeds to the cabinet power distribution unit (CDU).

Read More

Topics: power chain, remote power panel, Data Center, CDU, Power, Server Technology

Explore Our Blog

See all
email-header_opt-in-verification-rd02_v01

Latest Posts

Follow Me