<iframe src="//www.googletagmanager.com/ns.html?id=GTM-WHST8N" height="0" width="0" style="display:none;visibility:hidden">

Stay Powered Blog

PDU API: Open, Easy and Efficient

Posted by Calvin Nicholson on Aug 16, 2018 7:05:00 AM

 

Read More

Topics: Helpful Features, power distribution and monitoring

Top Reasons to Use Switched PDUs in Your Data Center

Posted by Josh Schaap on Jun 5, 2018 11:10:00 AM

Originally posted July 1, 2016, Updated June 05, 2018

Read More

Topics: Switched PDU, Helpful Features, switched rack PDU, network controlled power strip

Rack PDUs:  Making the Choices less of a Challenge

Posted by RJ Tee on Apr 30, 2018 1:43:04 PM

While in previous blogs we’ve talked about the advantages of customization and having so many PDU options to choose from, now might be a good time to keep it simple.  Server Technology is in the business of meeting complex power needs for every customer’s equipment and data demands.  But we would be remiss if we didn’t address those needs in the simplest and most straightforward way possible.

Read More

Topics: Helpful Features, PDU, rack PDU, Servertech PDU

Don’t Have A Cow About Load Balancing, Man

Posted by Erik Stabile on Mar 14, 2018 4:45:00 PM

Originally Posted Sep 30, 2015, Updated Mar, 14, 2018

Read More

Topics: Helpful Features, smart PDU, 3 phase PDU, server power distribution

On the Benefits of Alternating Phase

Posted by RJ Tee on Feb 9, 2018 10:49:00 AM

Originally Posted on Oct 10, 2017 - Updated Feb 09, 2018

We’ve extolled the virtues of single phase 60A power distribution to the rack.  But there are still may situations in which a three phase deployment is required to power the needs of racks that consume 12kW or more.  In other words, situations that begin with ‘high’ and end with ‘density.’

Read More

Topics: 3 Phase power, Alternating phase, Helpful Features, 3 phase PDU

Making Light Work of Configuring with Zero Touch Provisioning

Posted by RJ Tee on Feb 6, 2018 10:05:00 AM

Read More

Topics: Helpful Features, intelligent PDU, Server Technology, IP controlled power strip

Latest Posts

email-header_opt-in-verification-rd02_v01

Follow Me

All Categories

See all