<iframe src="//www.googletagmanager.com/ns.html?id=GTM-WHST8N" height="0" width="0" style="display:none;visibility:hidden">

Stay Powered Blog

HDOT Cx in the Realm of Great Ideas: Part 1

Posted by RJ Tee on Sep 17, 2018 11:02:42 AM

blog-header+hdot-cx_in-the-realm-of-great-ideas_v01

AML-11372_7644022_mutable_color

While the Server Technology engineers here in Reno are a little more on the ball than Frank and Earnest, the newly launched power distribution unit we’ve dubbed ‘HDOT Cx’ could arguably be a turning point in network PDU history. 

Frank:  This claim about the HDOT Cx, it is bold. 

Earnest:  Sí, señor. 

 To start our three part series about great ideas, it is only fair to introduce you first to the new

HDOT Cx outlet.

 

 HDOT Cx, meet the reader.  Reader, meet the new HDOT Cx:

  •  The Cx outlet is a hybrid device that can function as either a C13 or a C19 outlet. With no additional parts, you can plug in a C14 or C20 cord into one outlet.Outlets-Group of 3_RGB

    HDOT Cx Outlets

  • This innovative design reduces complexity within the selection process. It limits the need to purchase a new set of PDUs when equipment changes, resulting in lower end costs

Now, tell me that’s not a great idea!  If you are not creeped out by the term ‘HDOT Cx’, check out the newly-released solution video and see why Server Technology is the home of award-winning density solutions.  At Server Technology, we create great ideas to help our customers Stay Powered, Be Supported and Get Ahead.     

FRANK & ERNEST © Thaves. Used By permission of ANDREWS MCMEEL SYNDICATION. All rights reserved.

Topics: Server Technolgy, Power Distribution Unit, network pdu, For Fun

Get In Touch

Latest Posts

Follow Me