<iframe src="//www.googletagmanager.com/ns.html?id=GTM-WHST8N" height="0" width="0" style="display:none;visibility:hidden">

Stay Powered Blog

Five Great Things You Can do with SPM

Posted by Josh Schaap on Jan 9, 2017 12:05:41 PM

5spm-01-01.jpg

Data center power management has never been easier thanks to Server Technology’s Sentry Power Manager (SPM) platform.  SPM is a fully-automated, Web-based solution that gives operators real-time visibility into the network and the ability to switch from any location. Using SPM, operators can more effectively manage their infrastructure — be it onsite or distributed — and fast-track power and cost reductions.  

SPM works in conjunction with most of Server Technology’s intelligent data center power distribution units (PDUs) including Smart and Switched, as well as Smart POPS and Switched POPs devices. These PDUs offer various levels of control and insight into each cabinet’s electricity consumption. And it all comes together in the SPM platform, the system’s central operational hub which can be accessed from any Web interface.

Here are five great ways that you can use SPM to improve operations in your facility: 

  1. Create reports: One of SPM’s most powerful tools is its reporting feature. This solution makes it possible to schedule and run custom power scans across specific areas of the network, at any time. This is useful for tasks like finding the time of the week when your data center consumes the most power. You can drill down into any part of the network that is connected to a smart PDU and gain access to critical performance metrics. Once a scan is complete, a full report can be easily generated and exported to team members so that everyone has a thorough understanding of how the data center is consuming power. It’s a much more efficient way to generate data than by manually combing the network for information and compiling it into spreadsheets. Spreadsheets are error-prone and can can be tampered with, while SPM, in contrast, is highly secure. The platform comes with strong authentication settings to ensure that only approved individuals can access the data. Multiple users can access SPM at the same time, making it easier for employees to work together when performing maintenance.
  1. Control your environment: SPM will keep a close watch on your facility’s temperature and humidity levels, to ensure operating conditions are optimal for your setup. SPM will alert you if action needs to be taken. Also, using this technology you can safely experiment with different environmental settings to reduce total energy costs. The platform can set minimum or maximum temperature thresholds, and it can provide critical data that you can use to see if your cost reduction strategies are paying off over time.
  1. Save time during firmware upgrades: Intelligent PDUs have one small drawback: They need to be upgraded with new firmware from time to time. This process can eat up precious hours during the week. With SPM, you can schedule firmware upgrades to automatically take place during the off hours on nights and weekends, so that updates will be complete by the time the devices are needed during the week. It’s also one less task you will have to worry about!
  1. Conserve resources: In a typical data center, about 40 - 60 percent of all power goes to the cabinets. So it’s important to ensure that the energy is being used effectively, and not being wasted on things like idle servers. SPM makes it possible to ensure that power is flowing properly across the network—meaning in a balanced and organized way.
  1. Ensure rack redundancy: In the past, operators were forced to perform network stress tests to see how they would perform during unplanned outages. Servers would have to be manually shut down and rebooted. This was a time-consuming, and somewhat risky process. SPM improves this process by automatically scanning the network to ensure that all systems are functioning properly. No shutdowns are required.

Ultimately, SPM will provide peace of mind and a greater sense of security in your data center. By using SPM, you can ensure that your data center’s most important foundational resource, electricity, is being used in the best possible manner. You and your colleagues will no longer have to waste time on menial power management research. This product will free you to take on higher-level projects.  

SPM, it should be noted, is especially useful for federal agencies which now must comply with cost and power reduction mandates. Federally-owned data centers must now track the resources they use and prove they are taking measures to slash costs and become more environmentally-friendly. Server Technology’s solutions are TAA compliant, and are being actively used in many federal agencies today.

Don’t wait to improve energy efficiency in your data center.

Topics: SPM, Sentry Power Manager

Get In Touch

Latest Posts

Follow Me