<iframe src="//www.googletagmanager.com/ns.html?id=GTM-WHST8N" height="0" width="0" style="display:none;visibility:hidden">

Stay Powered Blog

Dilbert’s Top 5 Lessons for the Data Center: Number Four

Posted by Calvin Nicholson on Jun 5, 2015 7:00:00 AM

Dilbert Lessons for the data center is a five part series. Check back for more! 

Number 4) There is a lot of value in server virtualization and consolidation projects:

  • This is a great time to update the cabinet or cabinet PDU at the same time to leverage new functionality and features.
  • Though a PDU is part of the critical physical infrastructure it cannot last forever especially as hot aisle temperatures continue to rise.
  • Great time to also look at 3-Phase 400V power solutions (230 or 240V to the device) as another way to increase efficiency in your data center.
  • If you go 3-Phase then an alternating phase PDU will greatly reduce the length of the required power cords and increase air flow within your cabinet.
  • Existing POPS PDU’s combined with software tools easily allow the user to determine which servers are zombies and which are actually doing useful work.
  • Also a great time to update to new servers with more efficient power supplies for greater overall cost savings.

dt_c080212

Number Three

Topics: data center consolidation, server virtualization

Get In Touch

Latest Posts

Follow Me